SLVSGG5C november 2021 – april 2023 TPS2597
PRODUCTION DATA
In the case of a short-circuit and overload current limit when the device interrupts current flow, the input inductance generates a positive voltage spike on the input, and the output inductance generates a negative voltage spike on the output. The peak amplitude of voltage spikes (transients) is dependent on the value of inductance in series to the input or output of the device. Such transients can exceed the absolute maximum ratings of the device if steps are not taken to address the issue. Typical methods for addressing transients include:
Use Equation 19 to estimate the approximate value of input capacitance:
where
Figure 9-10 shows the circuit implementation with optional protection components.