SLVSGI0C September 2022 – June 2024 DRV8411
PRODUCTION DATA
In the parallel bridge interface, the DRV8411 is configured to drive a higher current brushed-DC (BDC) motor by connecting the driver outputs in parallel to reduce the RDS(ON) by a factor of two. Figure 8-3 shows an example of how to connect the pins on the device. To use parallel bridge interface operation, connect AIN1 and BIN1 to the same control signal, IN1, and connect AIN2 and BIN2 to the same control signal, IN2. Similarly, connect AOUT1 and BOUT1 to the same output node, OUT1, and connect AOUT2 and BOUT2 to the same output node, OUT2. AISEN and BISEN must be connected to the same ground plane.
This mode can deliver the full functionality of the BDC motor control with all four modes (forward, reverse, coast, and brake mode). Table 8-4 shows the control interface states in parallel mode.
nSLEEP | IN1 (AIN1 & BIN1) | IN2 (AIN2 & BIN2) | OUT1 (AOUT1 & BOUT1 | OUT2 (AOUT2 & BOUT2) | DESCRIPTION |
---|---|---|---|---|---|
0 | X | X | High-Z | High-Z | Low-power sleep mode |
1 | 0 | 0 | High-Z | High-Z | Coast; H-bridge disabled to High-Z |
1 | 0 | 1 | L | H | Reverse (Current OUT2 → OUT1) |
1 | 1 | 0 | H | L | Forward (Current OUT1 → OUT2) |
1 | 1 | 1 | L | L | Brake; low-side slow decay |