Figure 4-2 is the
recommended test setup to evaluate the TPS53319EVM-136. Working at an ESD
workstation, make sure that any wrist straps, bootstraps, or mats are connected
referencing the user to earth ground before power is applied to the EVM.
Input Connections:
- Prior to connecting the DC input source
VIN, it is advisable to limit the source current from VIN to 10-A
maximum. Make sure VIN is initially set to 0 V and connected as shown in Figure 4-2.
- Connect a voltmeter V1 at TP1 (VIN)
and TP10 (GND) to measure the input voltage.
- Connect a current meter A1 to measure the input current.
Output Connections
- Connect the load to J2 and set the load to
constant resistance mode to sink 0 ADC before VIN is
applied.
- Connect a voltmeter V2 at TP2 (VOUT)
and TP11 (GND) to measure the output voltage.