SLVU735A June 2012 – February 2022 TPS51225
Make all switcher selections before applying power to the EVM. Configure this EVM per the following:
Enable1 Selection
The EN1 pin can be set by S1.
Default setting: S1 to OFF to disable the Output1
Switcher set to | SKIPSEL Selection |
ON | Enable the Output1 |
OFF | Disable the Output1 |
Enable2 Selection
Default setting: S2 to OFF to disable the Output2
Switcher set to | Enable Selection |
ON | Enable the Output2 |
OFF | Disable the Output2 |