SLVUAW9C September 2016 – February 2020 UCD90320
This Read/Write Byte common command allows the user to read/write a byte value to RAM in the device. This RAM value is reset to a known value (0) when the controller is reset. By monitoring this value, the user is able to tell that the controller has been reset during operation.
Note that this parameter is not stored to nonvolatile Default Store memory when the STORE_DEFAULT_ALL command is issued.