SLVUAW9C September 2016 – February 2020 UCD90320
The Page Mask consists of three configuration bytes. The bits are defined as follows:
Bit | 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
Purpose | PAGE31 | PAGE30 | PAGE29 | PAGE28 | PAGE27 | PAGE26 | PAGE25 | PAGE24 |
spacer | ||||||||
Bit | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
Purpose | PAGE23 | PAGE22 | PAGE21 | PAGE20 | PAGE19 | PAGE18 | PAGE17 | PAGE16 |
spacer | ||||||||
Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
Purpose | PAGE15 | PAGE14 | PAGE13 | PAGE12 | PAGE11 | PAGE10 | PAGE9 | PAGE8 |
spacer | ||||||||
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Purpose | PAGE7 | PAGE6 | PAGE5 | PAGE4 | PAGE3 | PAGE2 | PAGE1 | PAGE0 |
Each selects which pages are to be used in a given fault pin. Setting the bit associated with a given page to 1 enables the associated faults of that page. If the bit associated with a page is set to 0, the faults for page have no effect on the fault pin output.
The following faults have the impact on the fault pin:
RESEQUENCE_ERROR | SEQ_ON_TIMEOUT | SEQ_OFF_TIMEOUT | OT_FAULT | IOUT_OC_FAULT |
IOUT_UC_FAULT | VOUT_UV_FAULT | VOUT_OV_FAULT | TON_MAX_FAULT |