SLVUAW9C September 2016 – February 2020 UCD90320
The SEQ_TIMEOUT command (D0h) defines a window during which an external event is expected to occur. That event is defined by the Input Pin selected by this byte (see Table 66). The pin is ignored if the value of this byte is zero or the SEQ_TIMEOUT window is set to 0.
Value | Description |
---|---|
0 | Unused |
1 | GPI_0 Pin Configuration |
2 | GPI_1 Pin Configuration |
3 | GPI_2 Pin Configuration |
4 | GPI_3 Pin Configuration |
5 | GPI_4 Pin Configuration |
6 | GPI_5 Pin Configuration |
7 | GPI_6 Pin Configuration |
8 | GPI_7 Pin Configuration |
9 | GPI_8 Pin Configuration |
10 | GPI_9 Pin Configuration |
11 | GPI_10 Pin Configuration |
12 | GPI_11 Pin Configuration |
13 | GPI_12 Pin Configuration |
14 | GPI_13 Pin Configuration |
15 | GPI_14 Pin Configuration |
16 | GPI_15 Pin Configuration |
17 | GPI_16 Pin Configuration |
18 | GPI_17 Pin Configuration |
19 | GPI_18 Pin Configuration |
20 | GPI_19 Pin Configuration |
21 | GPI_20 Pin Configuration |
22 | GPI_21 Pin Configuration |
23 | GPI_22 Pin Configuration |
24 | GPI_23 Pin Configuration |
25 | GPI_24 Pin Configuration |
26 | GPI_25 Pin Configuration |
27 | GPI_26 Pin Configuration |
28 | GPI_27 Pin Configuration |
29 | GPI_28 Pin Configuration |
30 | GPI_29 Pin Configuration |
31 | GPI_30 Pin Configuration |
32 | GPI_31 Pin Configuration |
33-255 | Invalid |