This document is a quick guideline to help the user perform a schematics review to achieve the best performance. This document does not apply to the UCD9080 and UCD9081 devices.
The UCD90xxx family of digital power supply sequencers, also known as system health monitors are flexible and powerful enough to meet users sequencing, monitoring, margining and other needs. The entire family of devices are designed to have similar behaviors, with a different number of rails or some other minor features. Users only need to learn how to use the device once, and can then seamlessly switch to other devices within the family that best fit their future designs. This document is a quick guideline to help user to perform a schematics review to achieve the best performance. This document does not apply to the UCD9080 and UCD9081 device.
If a brownout circuit is used, ensure that forward voltage of the selected Schottky diode does not trigger the brownout voltage threshold under operational temperature range. The pullup source for the RESET signal must be connected to the cathode side of the diode, if brownout circuitry is used.