This user’s guide describes the characteristics, setup, and use of the LP5036EVM Evaluation Module (EVM). This EVM helps the user evaluate the features of the Texas Instruments LP5036 device, which is an I2C bus-controlled, 36-channel, constant-current LED driver. This user’s guide includes setup instructions, a schematic diagram, a bill of materials, printed-circuit board layout drawings, and software instructions.
The LP5036EVM can be converted for testing the LP5030 device by removing the factory-installed device (U1) and replacing it with the LP5030 counterpart. Then when testing, select the corresponding LP5030 tag from the menu on the GUI home page (Figure 5) for the evaluation.
All trademarks are the property of their respective owners.
The LP5036EVM kit (Figure 1) contains:.
Figure 2 shows the key connectors used to operate LP5036EVM.
PARAMETER | RANGE |
---|---|
VCC | 3 V–5.5 V |
VLED | 3 V–5.5 V |
VMCU | 1.8 V, 3.3 V, 5 V |
Channel current | 35 mA (maximum) |
Note: Channel current is set at 20 mA when the LED supply voltage is 5 V. Although the LP5036 device can withstand 6-V maximum LED supply voltage with 35 mA per channel, make sure that the PCB thermal performance can meet the power dissipation requirement, because increased LED supply voltage increases channel output current.