All trademarks are the property of their respective owners.
TI's Evaluation Module LM74810EVM helps designers evaluate the operation and performance of the LM74810-Q1 ideal diode controller with switched output. This evaluation module demonstrates how LM74810-Q1 controls two N-channel power MOSFETs with ideal diode MOSFET connected first followed by second MOSFET for switched output and power path cut-off. LM74810-Q1 is a dual gate drive Ideal diode controller where the first gate drive DGATE controls an external N-channel MOSFET to emulate an ideal diode and the second gate drive HGATE controls another external N-Channel MOSFET to cutoff the power path when disabled or during an over voltage condition. Second MOSFET is can also be used to clamp the output during over voltage or load dump conditions.
High Current Warning: LM74810EVM is capable to handle 10 A of current and necessary safety precautions are required when using the EVM. EVM does not produce > 5-A current on its own, but passes the current from input power to the load.
For Class A performance during input micro-short test LV124 E-10, it is recommended to connect EN/UVLO, J5 pin 2 to J10 pin 1 or an external control using J5 pin 2.