SLVUBX5B August 2023 – February 2024 TPS25762-Q1 , TPS25772-Q1
The EEPROM device can be programmed with the Full Flash binary file generated using the GUI with a valid set of keys as detailed in Section 5.1.1. While the EEPROM on the TPS257xx-Q1 EVM can be programmed using the onboard TIVA MCU, it is also possible to use a standard EEPROM programmer interfaced with the proper pins on the EVM. Use of an EEPROM programmer can also be used when programming the EEPROM of a custom hardware design. This is required for the initial programming of a blank EEPROM.
For example, EEPROM programming can be done using the Total Phase™ Aardvark I2C/SPI™ Host Adapter. The following steps are required to use the programmer:
Once setup is completed, use the following steps to program the EEPROM: