Launch the GUI tool either through a web browser or locally as a desktop application following these steps:
- Navigate to TPS257XX-Q1-GUI using a supported web browser
- Click the Evaluate in the cloud button
- A new tab opens with the application launched
If the TI Cloud Agent is not already installed, instructions appear for installing the required software.
To download and install the application locally on the PC follow these steps:
- Navigate to TPS257XX-Q1-GUI using a supported web browser
- Click the Download button
- If required, select the application dashboard that has the correct tool displayed
- Click on the downwards-facing arrow on the bottom left side of the dashboard, and look towards the top set of links that appear. Select the operating system, and open the installer.
- Once the installer is open, follow the directions to install the GUI application
The TPS257xx-Q1-GUI application configuration tool provides users with the following capabilities:
- Generate application configuration settings in a binary file format
- Load configuration settings to the onboard EEPROM of the EVM
- Load configuration settings to an EVM (or custom hardware) along with security keys using the USB Type-C® port
- Save configuration settings in JSON format locally for future use