SLVUC07A December 2020 – May 2021 TPS543320
The TPS543320EVM is provided with input connectors, output connectors, and test points as shown in Table 3-1 and Table 3-2.
To support the minimum input voltage with the full rated load on both outputs with the default EVM, a power supply capable of supplying greater than 3 A must be connected to J8 through a pair of 20-AWG wires or better. Banana jacks J5 and J9 provide an alternative connection to input power supply.
For U1, the load must be connected to J2 and for U2, the load must be connected to J7. A pair of 20-AWG wires or better must be used for each connection. With the maximum current limit setting, the maximum load current capability is near 5 A before the TPS543320 goes into current limit. Wire lengths must be minimized to reduce losses in the wires.
Test point TP11 provides a place to monitor the VIN input voltage with TP19 providing a convenient ground reference. TP2 is used to monitor the output voltage of U1 with TP5 as the ground reference. TP15 is used to monitor the output voltage of U2 with TP17 as the ground reference.
If modifications are made to the TPS543320EVM, the input current may change. The input power supply and wires connecting the EVM to the power supply must be rated for the input current.
For the FSEL pin of the TPS543320 to detect and set the correct switching frequency, the pin must either detect the resistor to ground or an external clock must applied to the pin before enabling the regulator. If starting up without an external clock, to properly detect the FSEL resistor value connected to ground, the buffers on the EVM need to be in high impedance mode. The shunts on J15 and J16 must be removed to put the buffers in high impedance mode for startup without an external clock.
REFERENCE DESIGNATOR | NAME | RELATED IC | FUNCTION |
---|---|---|---|
J2 | VOUT | U1 | VOUT screw terminal to connect load to output |
J4 | EN_OFF | U1 | 2-pin header for enable. Add shunt to connect EN to ground and disable device. |
J5, J9 | VIN | Both | Banana jack for positive terminal and negative terminal of input power supply |
J7 | VOUT | U2 | VOUT screw terminal to connect load to output |
J8 | VIN | Both | VIN screw terminal to connect input voltage (see Table 1-1 for VIN range) |
J11 | RDIV_VIN | U2 | 2-pin header for enable divider. Remove shunt to disconnect EN pin divider for U2 from VIN. If J11 shunt is removed and J13 shunt is populated, U2 EN pin is pulled to ground through bottom resistor in divider disabling U2. |
J13 | EN_RDIV | U2 | 2-pin header to connect enable divider to U2. Remove shunt to float EN pin of U2 to use internal UVLO to enable U2. |
J14 | VOUT Select | U2 | VOUT selection header. Use shunt to set output voltage. See Table 2-1. |
J15 | ENSYNC_U1 | U1 | 2-pin header to connect U1 buffer output enable to ground. Populate shunt to enable output of buffer. Remove shunt to make buffer output high impedance. |
J16 | ENSYNC_U2 | U2 | 2-pin header to connect U2 buffer output enable to ground. Populate shunt to enable output of buffer. Remove shunt to make buffer output high impedance. |
J17 | FSEL Select | U2 | FSEL selection header. Use shunt to select FSEL resistor. See Table 2-2. |
J18 | MODE Select | U2 | MODE selection header. Use shunt to select MODE resistor. See Table 2-3. |
REFERENCE DESIGNATOR | NAME | RELATED IC | FUNCTION |
---|---|---|---|
TP1 | VIN_U1 | U1 | VIN test point. Use this for efficiency measurements. |
TP2 | VOUT_U1 | U1 | VOUT test point. Use this for efficiency, output regulation, and bode plot measurements. |
TP3 | SW_U1 | U1 | SW node solder mask opening |
TP4 | PGND_U1 | U1 | PGND test point |
TP5 | PGND_EFF_U1 | U1 | PGND test point. Use this for efficiency measurements. |
TP6 | PGOOD_U1 | U1 | PGOOD test point |
TP7 | EN_U1 | U1 | EN test point. If applying an external voltage, it must be kept below the absolute maximum voltage of the EN pin of 6 V. |
TP8 | AGND_U1 | U1 | AGND test point |
TP9 | BODE_U1 | U1 | Test point between voltage divider network and output voltage. Used for Bode plot measurements. |
TP10 | VOUT_U1 | U1 | SMB connector to measure output voltage. When using this test point, the scope should be set for 1-MΩ termination. When using 50-Ω termination, a 2:1 divider is created. |
TP11 | VIN | Both | VIN test point near input terminals |
TP12 | VIN_U2 | U2 | VIN test point. Use this for efficiency measurements. |
TP13 | SW_U2 | U2 | SW node solder mask opening |
TP14 | SW_U2 | U2 | SW node test point |
TP15 | VOUT_U2 | U2 | VOUT test point. Use this for efficiency, output regulation, and bode plot measurements. |
TP16 | PGND_U2 | U2 | PGND test point |
TP17 | PGND_EFF_U2 | U2 | PGND test point. Use this for efficiency measurements. |
TP18 | PGOOD_U2 | U2 | PGOOD test point |
TP19 | PGND | Both | PGND test point near input terminals |
TP20 | AGND_U2 | U2 | AGND test point |
TP21 | BP5_U2 | U2 | BP5 test point |
TP22 | BODE_U2 | U2 | Test point between voltage divider network and output voltage. Used for Bode plot measurements. |
TP23 | EN_U2 | U2 | EN test point. If you are applying an external voltage, it must be kept below the absolute maximum voltage of the EN pin of 6 V. |
TP24 | VO_ADJ | U2 | Test point for injecting current into the FB divider to adjust the DC output voltage or inject a step to FB to test OVP |
TP25 | VO_2NDSTG | U2 | Test point to measure output voltage after second stage filter if added to EVM. |
TP26 | SYNC | Both | SYNC test point. Supply an external clock to this test point to synchronize both regulators to it. |
TP27 | FSEL | U2 | FSEL test point |
TP28 | SW_U2 | U2 | SMB connector to measure SW node. When using this test point, the scope should be set for 50-Ω termination. The combination of 50-Ω termination and 450-Ω series resistance creates a 10:1 attenuation. |
TP29 | VOUT_U2 | U2 | SMB connector to measure output voltage. When using this test point, the scope should be set for 1-MΩ termination. When using 50-Ω termination, a 2:1 divider is created. |
TP30 | VO_2NDSTG | U2 | SMB connector to measure output voltage after second stage filter if added to EVM. When using this test point, the scope should be set for 1-MΩ termination. When using 50-Ω termination, a 2:1 divider is created. |
TP31 | FGEN | Both | Test point to connect function generator to load transient circuit. Slowly increase amplitude and vary slew rate of function generator for desired load step. |
TP32 | ISNS | Both | Test point to measure current in load transient circuit. Gain is 10 A/V. |
TP33 | PGND | Both | PGND test point for load transient circuit |
TP34 | MODE | U2 | MODE test point |