SLVUC50 April 2021 LM66200
The LM66200EVM is an evaluation module for the LM66200 low IQ ideal diode. The LM66200 is a dual-input, single-output device that automatically passes the higher of its two input voltage to the output. The low quiescent current makes the LM66200 ideal for systems with a battery supply as an input to extend the life of the battery when in use.