Use the following instructions to perform the
overvoltage protection test on channel 1:
Remove input TVS diodes.
Set the input supply voltage VIN to 12 V and current limit of 10 A. Apply the supply between VIN1 and PGND1 at connector J1 and enable the power supply.
Increase the input supply VIN from 12 V to 16 V and observe the waveforms using an oscilloscope.
Figure 5-6
shows overvoltage response of TPS25972x on the TPS2597EVM eFuse
evaluation board.
Figure 5-6 Overvoltage Protection Response of the
TPS25972x Device