The TPS65219EVM can be
configured as follows. The following sections outline how to configure the
TPS65219EVM for general experimentation.
- Configure regulator input supply
rails for the expected application using the jumpers indicated in the Supply
Voltage Setup.
- Configure the multi-function pins
externally using the mode configuration descriptions indicated in
Multi-Function pin setup. Please note that the default configuration
for regulator choice in SD or DDR voltage selection can differ for each
individual NVM configuration (polarity is configurable).
- Connect VSYS to a power supply
capable of supporting the application and enable the supply.
- If using a version of TPS65219
configured for First Supply Detection (FSD), then the power-up sequence is
executed as soon as a valid supply is connected to VSYS.