JP2 is used to set different MODE/S-CONF
configurations. MODE/S-CONF can be connected to VIN and GND as a traditional HIGH
or LOW level. R6 and R7 select the other device configurations including the
following:
Internal/external
feedback
Switching frequency
Output discharge
Auto PFM/PWM(with AEE) or
forced PWM options
The values of R6 and R7 can be changed per the user’s requirement.
While using the internal feedback (VSET)
configuration for the output voltage setting, either float the FB pin by
cutting the net tie (NT1) included on the back of the board or remove both
R1 and R2 for a 3.3-V output voltage. Other output voltage can be programmed
by removing R1 and changing the value of R2. Ensure the JP2 jumper is placed
correctly for proper operation with internal feedback.
WARNING: Do not set the MODE/S-CONF pin for external feedback if
either the net tie (NT1) is cut or R1 and R2 are removed. This can
cause damage to the device due to lack of external feedback
control.
Dynamic mode option is an advance feature that
allows MODE/S-CONF pin to actively switch between forced PWM and auto
PFM/PWM during operation, but this is only possible by driving the
MODE/S-CONF pin between VIN and GND. This feature provides the user with the
option of controlling if and when the device enters power save mode
(DCM).