SLVUCF2 March 2022 TPS55289
The JP8 jumper is for the internal LDO or external VCC selection. By default, the jumper is set to the VCC position and the device selects an internal LDO as the VCC source.
To minimize the power dissipation of the internal LDO when both input voltage and output voltage are high, an external 5-V power supply can be applied at the VCC pin to supply the TPS55289. Place a jumper across EXTVCC and AGND to set the device VCC source externally. The external 5-V power supply must have at least 100-mA output current capability and must be within the 4.75-V to 5.5-V regulation range.