SLVUCF2 March   2022 TPS55289

 

  1.   Trademarks
  2. 1Introduction
    1. 1.1 Performance Specification
    2. 1.2 Modification
      1. 1.2.1 Modification
  3. 2Connector, Test Point, and Jumper Descriptions
    1. 2.1 Connector and Test Point Descriptions
    2. 2.2 Jumper Configuration
      1. 2.2.1 JP1 (ENABLE)
      2. 2.2.2 JP6 (SYNC)
      3. 2.2.3 JP7 (I2C Target Address Selection)
      4. 2.2.4 JP8 (Internal or External VCC Selection)
      5. 2.2.5 JP9 and JP10 (External Feedback and Internal Feedback Selection)
  4. 3Test Procedure
  5. 4Software User Interface
    1. 4.1 Install USB2ANY Explorer
    2. 4.2 GUI Installation
    3. 4.3 Interface Hardware Setup
    4. 4.4 User Interface Operation
    5. 4.5 Register Map Screen
  6. 5Schematic, Bill of Materials, and Board Layout
    1. 5.1 Schematic
    2. 5.2 List of Materials
    3. 5.3 Board Layout

User Interface Operation

The TPS55289EVM board can be enabled to work by the following steps:

  1. Set JP1 to the ON position. Turn on the power supply.
  2. Open the TPS55289EVM GUI.
  3. Click the auto connect button on the target address widget (Figure 4-2). It will automatically check for target addresses (0x74, 0x75) and connect the GUI with the device. After the GUI and device are connected, the GUI reads all eight registers and shows a notification (Figure 4-3).
    GUID-42AFF60E-EF40-460C-AA1B-FAB2F8398AE6-low.png Figure 4-2 GUI Auto Connect Button
    GUID-6E02E63B-5347-4974-8C02-6AB6A6F50695-low.png Figure 4-3 GUI Auto Connect Notification
  4. Click the start button. It will show the GUI user interface of TPS55289EVM-093 (Figure 4-4).
    Figure 4-4 GUI User Interface of TPS55289EVM-093
  5. Click the Enable button (Figure 4-5). The default output voltage is 5 V.
    Figure 4-5 ENABLE Button
  6. Set the output voltage, current limit point, and so forth according to the design target. If the maximum load current is ≥ 5 A, uncheck the ‘Enable Current Limit’ check box or increase the current limit value (Figure 4-6).
    GUID-4C51F0DF-B61D-4ED7-AEF1-4C6D98CFF107-low.png Figure 4-6 Output Current Limit Point Setting