SLVUCG0 May 2022 TPSI3052-Q1
To configure the EVM for two-wire mode, the following changes must be made:
Figure 3-2 provides a visual representation of how to configure the board for the two-wire mode:
J4-Header | IEN |
---|---|
PXFR #1 (7.32 kΩ) | 1.9 mA |
PXFR #2 (20 kΩ) | 6.7 mA |
Figure 3-3 shows the powering up delay from EN rising to VDDM and VDDP rising using the highest power transfer PXFR #2 (20 kΩ) in two-wire mode. The power up delay is directly related to the power transfer selection and to the capacitors from VDDH to VDDM and VDDM to VSSS. The delay from EN to VDDM is 2 ms and the delay from EN to VDDH is 1.83 ms. Figure 3-3 shows the delay from EN rising to VDRV rising using the highest power transfer PXFR #2 (20 kΩ) in two-wire mode. The delay from EN to VDRV is 3.533 ms. Figure 3-5 shows the delay from EN falling to VDRV falling. The delay is 2.463 us.