The following procedure outlines the steps to be
taken for using the TLVM23625EVM. Use this section in conjuction with Test
Setup to correctly setup the EVM.
- Determine the output voltage that is to be
evaluated, then reference Setup
Procedure. This table provides the recommended jumper
configurations.
- After making any required changes, confirm that the output voltage is within a couple percent of the set output voltage.
- Verify the performance of the EVM and compare with applicable curves within this user's guide.
- Consult on e2e if there are concerns in the evaluation of this device.
Table 2-1 Suggested Switching Frequency SettingsVOUT (V) | Suggested Frequency |
---|
1.8 | 300 kHz |
2.5 | 800 kHz |
3.3 | 800 kHz |
5 | 1 MHz (J4: 3 – 4) *2.2 MHz can improve transient response for given output capacitance. |