SLVUCM2A january 2023 – july 2023 TPSF12C3 , TPSF12C3-Q1
The EVM daughter-card connects to the main EMI filter board through header J1. The sense and inject capacitors, along with a robust ground connection, interfaces the low-voltage EVM to the high-voltage power lines.
Header J1 provides an interface through terminals S1, S2, S3, S4, INJ and GND, as described in Table 3-1. Connect S1, S2, S3 and S4 to the sense capacitors as shown in Figure 3-3. Connect the opposite terminals of the sense capacitors to the Live and Neutral power lines between the CM chokes, LCM1 and LCM2. Connect INJ to the inject capacitor, designated as CINJ, whose opposite terminal then connects to any power line as shown. The X-capacitors at this position, designated as CX4, CX5 and CX6, set a low impedance between the power lines from a CM standpoint – this means that a single inject capacitor is adequate for current injection. Finally, connect a nominal 12-V bias supply from VDD to GND to power the AEF circuit. The GND attachment point on the filter board corresponds to where the Y-capacitors in a passive design normally connect.
Refer to the diagram of Figure 3-3 for an example of component placement on a filter board (this design has the AEF components mounted directly on the PCB).