SLVUCM5 july 2023 TPS6521905 , TPS6521905-Q1
The TPS6521905 has the default I2C address configured as 0x30. This configuration can be changed if needed by searching for register I2C_ADDRESS_REG in the register map of the TPS65219_GUI and changing the default 0x30 address as shown in Figure 4-9. Once the register is changed, the new value must be saved into the NVM by writing 0x0A to register 0x34.
Register Address | Bit | |
---|---|---|
Bit# | Field Name | |
0x26 | 6-0 | I2C_ADDRESS_REG |