SLVUCM5 july 2023 TPS6521905 , TPS6521905-Q1
The diagram shown in Figure 6-1 describes the process to load a pre-configured NVM file (.CSV or .JSON extension) into the PMIC NVM. The soldered down EVM (TPS65219EVM) is used as a reference but the socketed EVM can be used as well. The TPS6521905 product page has multiple NVM files that are pre-configured to meet the requirements of specific processors or SoCs. TI's customers can reuse these files to re-program the PMICs on their production line or by working with a distributor.