SLVUCN7 January   2023

 

  1.   TPS61299EVM-103 Evaluation Module
  2.   Trademarks
  3. 1Schematic
  4. 2Bill of Materials
  5. 3Board Layout

TPS61299EVM-103 Evaluation Module

This user's guide describes the schematic, layout, bill of materials (BOM), and setup of the evaluation module (EVM) for the TPS61299, which outputs a fixed 5 V in a WCSP package. The input voltage of the EVM is from 0.7 V to 5.5 V. The output current mainly depends on the input voltage, because the inductor peak current is limited at typical 1.2 A. The EVM supports typical 0.8A from a 3.6-V input voltage.