Now that the EVM hardware setup and GUI installation is complete, the EVM can now be connected to the GUI. The following steps outline how to connect the EVM to GUI:
- With the EVM connected to the PC, open the GUI.
The home page is shown in Figure 4-2.
-
- Program EVM with latest software by clicking on
File -> Program Device. (See Figure 4-3).
This needs to be done
the first time the user sets up the EVM, as a software update can have been
released since the EVM was initially programmed.
-
- Select the appropriate GUI variant from the five
options for the EVM (Figure 4-3).
-
- The GUI attempts to connect with EVM. The GUI
displays the following once successfully connected. If there is no successful
connection, then double check hardware setup is correct following steps in Section 2.4.
-
- Once successfully connected, click on Quick
Start to open the QuickStart page, or Dashboard or
Driver Control (DRV8213EVM) to open the main control page.
- The GUI setup is now complete. The following
section provides an overview of the GUI and how to use the GUI to control
EVM.