Ensure that the TPSI2072Q1EVM has the following setting on the jumpers:
- J7 – Shunt is connecting EN1 and EN1_EXT.
- J9 – Shunt is connecting EN2 and EN2_EXT.
- If not using a waveform generator as shown above, alternate setting the shunts to be between VDD and EN1/EN2. This action causes EN1/EN2 to be high when VDD is powered.