SLVUCP4 November 2023
The TPS25730EVM provides device status information of the TPS25730 using LEDs that correspond to GPIO events of the TPS25730. Each LED has the corresponding event printed to the left when the TPS25730EVM is oriented with TPS25730EVM readable.
GPIO Event | Description | Conditions for LED on |
---|---|---|
SINK_EN | Indicates when PPHV is enabled. Can be used for GPIO control of an external power path. | PPHV is disabled. |
PLUG_FLIP | Indicates the orientation of the USB-C plug. | Plug is upside-down. |
DBG_ACC | Indicates whether or not a debug accessory is connected. | Debug accessory is connected. |
PLUG_EVENT | Indicates a connection to a source device via a USB-C plug. | The LED turns on when connected. |
CAP_MIS | Indicates a mismatch in capabilities between the connected source and the TPS25730. | The LED blinks when a capabilities mismatch occurs. |
Each switch set must have only one of the eight switches in the on position, for a total of four switches in the ON position for a successful configuration. The table below shows which ADCIN pin configures which setting. Please note that ADCIN3 and ADCIN4 together determine operating current and maximum current based on the combination of the two inputs. ADCIN3 alone does not directly map to operating current and ADCIN4 does not map directly to maximum current.
ADCINx Pin | Corresponding Setting |
---|---|
ADCIN1 | Minimum voltage |
ADCIN2 | Maximum voltage |
ADCIN3 & ADCIN4 | Operating current and maximum current |
Each labeled switch number on the TPS25730EVM switch sets corresponds to an ADCIN decoded value, shown in the table below.
ADCIN Switch Number | ADCIN Decoded Value |
---|---|
1 | 0 |
2 | 1 |
3 | 2 |
4 | 3 |
5 | 4 |
6 | 5 |
7 | 6 |
8 | 7 |