SLVUCP9A November 2023 – March 2024 TPS25751
The required software is available at the TI Gallery, and is run from the web browser, provided that Google Chrome™, Firefox®, or Safari ®is used. If this is desired, then TI Cloud Agent needs to be installed as a browser extension as well as on the PC. When the application is launched, instructions appears for installing TI Cloud Agent. The software can also be run natively on the PC. If this is desired, then GUI Composer Runtime needs to be installed natively. To install GUI Composer Runtime, click on the downwards-facing arrow inside one of the applications listed in the Gallery, and look towards the bottom set of links that appear. After selecting the native operating system, open the installer and follow the prompts to install the program.