SLVUCP9A November 2023 – March 2024 TPS25751
To generate a VIF file of the current tool settings including the current configuration of the device as indicated by the form, click on the Export drop-down button on the top-right side of the tool and click on Generate VIF file. This automatically generates a VIF file to the default save directory on the user's computer. The VIF file is required for Compliance Testing specified by the USB Power-Delivery Certification Process. For more information on compliance testing, refer to USB Power Delivery - Compliance Tests Application Note.