SLVUCU8 January 2024
In the U1 design, the output voltage is set by the resistor divider network of R2 (RFBT) and R6 (RFBB). R6 is fixed at 8.25 kΩ to set the FB divider current at approximately 61 µA. The output voltage is set to 0.8V as default. To change the output voltage of the EVM, the value of resistor R2 must change. Changing the value of R2 can change the output voltage above the 0.5-V reference voltage (VREF). The value of R2 for a specific output voltage can be calculated using Equation 1.
In the U2 design, the output voltage is set by the resistor divider network of R15 (RFBT) and R12 (RFBB). R15 is fixed at 8.25 kΩ to set the FB divider current at approximately 61 µA. The output voltage is set to 0.8V as default. To change the output voltage of the EVM, the value of resistor R12 must change. Changing the value of R12 can change the output voltage above the 0.5-V reference voltage (VREF). The value of R12 for a specific output voltage can be calculated using Equation 1. After changing R12, the feed forward capacitor (C51) also needs to be changed.