Use the following instructions to perform the
persistent over-current test on TPS1685 eFuse:
- Configure the Jumper J2 to an appropriate
position to obtain the required overcurrent blanking period (tTIMER) as per
7.
- Configure the Jumper J6 position to the
desired reference voltage for overcurrent protection and active current sharing as
mentioned in 7.
- Configure the Jumper J3 in a good
position to set the required circuit breaker threshold (IOCP) as per 7.
- Configure the Jumper J7 in a good
position to set the required scalable fast-trip threshold (ISFT) as per 7.
- Set the input supply voltage VIN to 12V
and the current limit of 200A.
- Connect the power supply between VIN
(connector T1) and PGND (connector T3) and enable the power supply.
- Now apply an overload in the range of
IOCP andlt; ILOAD andlt; ISFT between VOUT (connector
T2) and PGND (connector T3) for a time duration more than tTIMER decided by
using jumper J2.
- Observe the waveforms using an
oscilloscope.
The circuit breaker response of TPS1685 eFuse on TPS1685EVM Evaluation Board with two
devices in parallel is shown in Figure 3-8.