Use the following instructions to perform the output hot short test:
- Set the input supply voltage VIN to 54V and connect the power supply between
VIN (connector T1) and PGND (Connector T3).
- Configure the Jumper J7 in a good position to set the required scalable
fast-trip threshold (ISFT) as per 7.
- Turn ON the power supply to power up the
EVM.
- Short the output of the device for example, VOUT (connector T2) to PGND
(connector T3) through a short cable.
- Observe the waveforms using an oscilloscope.
The test waveforms of output hot short on the
TPS1685EVM with two TPS1685 eFuses in parallel are shown in Figure 3-10 and Figure 3-10.
Note: Make sure there is sufficient input
capacitor to eliminate voltage dips at the input. A combination of electrolytic and ceramic
capacitors are preferred. With these capacitors, a large current can be provided for a short
period of time during short-circuit.
To obtain
repeatable and similar short-circuit testing results is very difficult. The following
contributes to the variation in results:
- Source bypassing
- Input leads
- Board layout
- Component selection
- Output shorting method
- Relative location of the short
- Instrumentation
The actual short exhibits a certain degree of randomness because the short microscopically
bounces and arcs. Make sure that configuration and methods are used to obtain realistic
results. Hence, do not expect to see waveforms exactly like the waveforms in this user's
guide because every setup is different.