Use the following instructions to observe the Quick Output Discharge (QOD) functionality:
- Set the input supply voltage VIN to 54V and current limit to 10A. Turn ON the
power supply.
- Use the switch SW1 to connect the EN/UVLO pin to ground to do power cycling.
- Use the switch SW2 to enable the QOD by making the voltage at EN/UVLO pin
approx. 1.1V.
- Observe the waveforms of VIN (TP1), VOUT (TP2), EN (TP3), and SWEN (TP4) using an oscilloscope.
The turn-off performance of the TPS1685 eFuse with
QOD enabled is shown in Figure 3-11. The turn-off performance with QOD disabled on the TPS1685EVMuse Evaluation Board is
shown in Figure 3-12.
Figure 3-11 QOD Enabled on TPS1685 eFuse
(VIN = 54V, COUT = 1mF, and EN Pulled Low to 1V) Figure 3-12 QOD Disabled on TPS1685 eFuse
(VIN = 54V, COUT = 1mF, and EN Pulled Low to 0V)