The TPS55287Q1EVM board can be enabled for
operation by the following steps:
- Set JP1 to the ON position. Turn on the power supply.
- Open the GUI.
- Click the Auto Connect button on the
target address widget (Figure 4-2). This automatically checks for target addresses (0x74, 0x75) and connect the
GUI with the device. After the GUI and device are connected, the GUI reads all
eight registers and shows a notification (Figure 4-3).
- Click the Start button. This shows the GUI
user interface of TPS55287Q1EVM-085 (Figure 4-4).
- Click the Enable button (Figure 4-5). The default output voltage is 5V.
- Set the output voltage,
current limit point, and so forth according to the design target. If the maximum
load current is ≥ 2.5A, then uncheck the Enable Current Limit check box
or increase the current limit value (Figure 4-6).