SLVUCZ9 July 2024 DRV81004-Q1 , DRV81008-Q1 , DRV81602-Q1 , DRV81620-Q1
The DRV81xxx-Q1 EVM connects to a local computer USB port through a USB-A to Micro-USB cable. A 3.3V LDO generates a 3.3V rail on the EVM from the USB 5V supply which powers the microcontroller. The J8 terminal can be used to provide the supply voltage (VM) of the device. Another 3.3V LDO powered from Vm generates the VDD required by the device in the EVM. Certain EVMs require jumper configurations to connect the device to the corresponding power rail. Be sure to verify jumper configurations before operation.