SLWU087E november 2013 – june 2023
After the board mode has been set, the user needs to select the device to be tested from the device selection drop-down menu. If the GUI is in ADC mode, clicking on the drop down arrow displays the ADC options available, as shown in Figure 3-26. If in DAC mode, the list displays available DACs.
Each device that has an ini file installed in the proper directory automatically has an entry in the device selection drop-down menu.
For TSW14J59revB Boards, after the Device Selection has been selected, click on OK on the "No firmware" message, the use the drop down arrow to select a device, as shown in Figure 3-27. When a Device Name is selected, the available device supported modes are listed in Figure 3-27. The user then can select a mode from the drop down.