This section describes the operation when testing with an ADC12DJ3200 EVM that has a JESD204B output interface.
- Power down the TSW14J58 EVM if an ADC EVM is not installed.
- Connect the ADC12DJ3200 EVM to the TSW14J58 EVM using the FMC connector.
- Provide +6 VDC connection to J2 of the TSW14J58 EVM and +5 VDC connection to J37 of the ADC12DJ3200 EVM.
- Connect a Micro-USB 3.0 cable to J1 and a Mini-USB 2.0 cable to J23 of the TSW14J58 EVM.
Connect a Mini-USB 2.0 cable to J31 of the ADC12DJ3200 EVM.
Power up the TSW14J58 and ADC12DJ3200 EVMs.
The TSW14J58 EVM connected to an ADC12DJ3200 EVM is shown in Figure 7-6.
Single Tone FFT Test
- The evaluation of the ADC12DJ3200 EVM requires programming the ADC, LMK04828, and LMX2582 devices. This process is easy using the ADC12DJxx00EVM GUI.
- Open the ADC12DJ3200 GUI and connect to the ADC.
- Select the onboard clock as the clocking source and choose a sampling rate from the drop down menu. This example uses a 3Gsps sampling rate.
- Choose JMODE3 as the Decimation and Serial Data Mode (Dual channel, 16 JESD204B lanes).
- Press the Program Clocks and ADC button and wait for programming to complete.
- Start the HSDC Pro GUI program. When the program starts, first connect to the TSW14J58 EVM board and then select the device ADC12DJ3200_JMODE3_2G_3G under the the Select ADC drop-down menu, as seen in Figure 7-7.
- When prompted by Load ADC Firmware?, select YES
- Select Single Tone FFT Test under Test Selection.
- Select the number of sample points (and resulting number of FFT bins) to be used. The example shown in Figure 7-8 has 65536 samples.
- Enter the ADC12DJ3200 sampling rate. The example shown in Figure 7-8 has the sample rate set at 3 Gsps.
- Enter the input frequency desired. The example shown in Figure 7-8 has the filtered input frequency set at 347 MHz and -3 dBFs on the HSDC Pro FFT plot.
- Select the channel the signal generator is connected to (channel B shown).
Press the Capture button on the HSDC Pro GUI.
Observe an FFT result similar to that of Figure 7-8.