SLWU087E november 2013 – june 2023
This section describes the operation when testing with an ADS5281 EVM that has a LVDS output interface.
To setup the GUI to run in the data capture mode, click on the “ADC” tab in the top left side of the GUI. Navigate to the device selection button located in the upper left side of the GUI, click on the drop down arrow, then select “ADS5281”. After clicking on this file, a pop-up opens asking “Do you want to update the Firmware for ADC”. Click on “Yes”. The firmware now starts loading, and takes approximately 20 seconds to complete. After the ADS5281 firmware load has completed, the FPGA_CONF_DONE LED turns on after the FPGA configured. The LEDs labeled USER_LED (0–7) are also on except for USER_LED4.
The user can now change other parameters and do another capture to observe the ADC outputs with different frequencies, amplitudes, and in other formats such as codes, or bits.
After the firmware is loaded, if the user clicks the drop down arrow in the device selection window, the GUI indicates which ADC EVMs can be used with this firmware load by adding a black diamond in front of the device name, as shown in Figure 4-3. If the user does not power down the TSW1400, any one of the devices with a black diamond can be tested without doing another firmware load. The devices supported with the current firmware are marked with a black diamond.