SLWU087E november 2013 – june 2023
For this test, at the top of the GUI, set the following parameters:
The pattern generation data file should match one of the Record Length’s to us the Rectangular window mode. If it does not, switch the window mode to another setting such as “Hanning”.
The display panel of the GUI is updated, showing the test data that is transmitted to the DAC EVM in both codes and frequency domain as shown in Figure 5-4.
Using a spectrum analyzer, verify that there is now a 25.1-MHz tone present on both SMA J2 (IOUTA2) and J3 (IOUTB2) of the DAC3152 EVM.
To shut down the GUI, click on the “File” tab in the upper right corner of the GUI and select “Exit” in the pop up window that opens. This will specify that the USB ports are released by the software.