SLWU094 March 2021
If an older version of the GUI has already been installed, make sure to uninstall it before loading a newer version. If the GUI detects that a newer version of the GUI is available online (http://www.ti.com/tool/DATACONVERTERPRO-SW), it will assist the user with downloading the latest version from the TI website. The GUI automatically interrogates the product website for the latest version every seven days but the latest version check can also be manually invoked through use of the pull-down menu Help→Check for updates.
When new TI high-speed data converter EVMs or JESD204C_B interface modes become available that are not currently supported by the latest release of HSDC Pro GUI, the HSDCProv_xpxx_Patch_setup executable, available on the TI website under the High Speed Data Converter Pro Software product folder (http://www.ti.com/tool/DATACONVERTERPRO-SW), will allow the user to add these to the GUI device list. After the patch has been downloaded, follow the on-screen instructions to run the patch. The software displays the files that will be added. After running the patch, open HSDC Pro and the new parts and modes will appear in the ADC and DAC device drop-down selection box. The patch is always specific to a core GUI version and will not work for a GUI version for which the patch was not explicitly created.