SLYA063A august 2022 – may 2023 DRV5032 , TMAG5131-Q1 , TMAG5170 , TMAG5170-Q1 , TMAG5170D-Q1 , TMAG5173-Q1 , TMAG5273
Designing a Hall-effect dial takes consideration to properly choose the magnet and sensor but eliminates a point-of-failure due to mechanical wear and tear. The reduction in potential failure points can be an essential improvement in applications such as a volume knob in an automotive center console or a selection dial on an appliance, since these products are difficult or costly to repair. Many magnet suppliers have tools for determining the magnet strength, which is used to determine the proper Hall-effect sensor.