SLYS035A September 2022 – September 2023 TMAG5173-Q1
PRODUCTION DATA
The TMAG5173-Q1 can be set in continuous conversion mode when OPERATING_MODE is set to 10b. Figure 8-1 shows a few examples of continuous conversion. The input magnetic field is processed in two steps. In the first step, the device spins the Hall sensor elements and integrates the sampled data. In the second step, the ADC block converts the analog signal into digital bits and stores in the corresponding result register. While the ADC starts processing the first magnetic sample, the spin block can start processing another magnetic sample. In this mode, the temperature data is taken at the beginning of each new conversion. This temperature data is used to compensate for the magnetic thermal drift.