SLYT835 March   2023

 

  1. 1Introduction
  2. 2A PSFB converter with an active clamp
  3. 3Active clamp leg design considerations
  4. 4Summary
  5. 5References

A PSFB converter with an active clamp

As shown in Figure 2-1, inserting an active clamp leg formed by a capacitor (CCL) and a MOSFET (QCL) before the output inductor enables active clamp leg current conduction within the effective duty-cycle (Deff) period, thus clamping the secondary winding voltage (VSEC) and rectifier voltage stress to the CCL voltage – VCL. In order to have low voltage stress on the output rectifier, you must select a large-enough CCL for low capacitor voltage ripple. A rule of thumb is to select the inductor-capacitor (LC) resonant period formed by Lr and CCL to be much longer than the switching period (Ts) [3] expressed by Equation 1:

Equation 1. 2 π N S N P 2 L r C C L T S

The rectifier voltage stress will clamp to around VINx NS/NP with the active snubber, which is about half of the voltage stress without any clamp circuit.

Unlike a passive snubber, an active snubber doesn’t dissipate the ringing energy on the power resistor. Instead, it circulates the energy in the LC resonant tank as a lossless snubber. When the output winding voltage becomes nonzero, energy will transfer from the primary winding to the secondary winding to energize the output inductor and conduct current through the QCL body diode, even if QCL isn’t turned on. Turning on QCL after its body has already conducted current will ensure zero voltage switching (ZVS) on QCL. Therefore, you can expect higher converter efficiency on a PSFB converter with an active snubber over a PSFB converter with a passive snubber in an identical specification.

Figure 2-1 A PSFB power stage with active clamp and key waveforms.