SLYT840 june   2023 INA333 , INA350

 

  1.   1
  2. 1Introduction
  3. 2Dual-supply circuits
  4. 3PCB layout
  5. 4Measurement results
  6. 5Conclusion

Dual-supply circuits

Figure 1 is a simplified schematic of a discrete, dual-supply IA using the Texas Instruments (TI) TLV9064 quad op-amp circuit. In this circuit, three of the four amplifier channels (A, B and C) are connected as a traditional three-op-amp IA. The reference voltage (VREF) connects to ground. With no use for the fourth channel, D, it is therefore connected as a buffer to mid-supply (ground) through a resistor for transient robustness. All resistors labeled “R” have a value of 10 kΩ; RG sets the differential gain. The differential input voltage is VIN+ − VIN– and the output voltage is VOUT. Some components, such as the load resistor (10 kΩ) and decoupling capacitors, are not shown. Drawing all circuits from a package perspective illustrates the number of external discrete components.

GUID-20230607-SS0I-C81C-WCPJ-DMPGS9MLJLPZ-low.svg Figure 1 A discrete dual-supply IA using a quad op amp.

Equation 1 gives the transfer function for this circuit:

Equation 1. V O U T = V I N + - V I N - × 1 + 20   k Ω R G

Designers will typically select a discrete IA when PCB area and performance are secondary to cost and gain range. TI’s TLV9064IRUCR op amp was selected for this comparison because it is a rail-to-rail input/output device (RRIO) with a wide bandwidth (10 MHz) and a low typical initial input offset voltage (VOS(typ) = 300 µV), and comes in a small package (RUC = X2QFN = 4 mm2). While there are less expensive RRIO quad op amps in RUC/X2QFN packages, they come at the expense of bandwidth and typical offset voltage.

To be consistent with the design priorities of discrete IAs, inexpensive ±1% tolerance, ±100-ppm/°C drift resistors were installed. Not only do these resistors differ in initial value, they will likely drift significantly over temperature. Since RG is external, the gain for this configuration is primarily limited by the input offset voltage of the op amps.

Figure 2 is a simplified schematic of the TI INA350ABS, a general-purpose dual-supply IA with an integrated RG. VREF connects to ground. This circuit integrates all resistors in the IA. The differential input voltage is VIN+ − VIN– and the output voltage is VOUT. Some components, such as the load resistor (10 kΩ) and decoupling capacitors, are not shown. The gain of the IA is set based on the switch connected to pin 1 (open = 20 V/V, closed = 10 V/V). In an actual application, the switch would not be present. To enable the device, connect pin 8 (SHDN) to V+ or leave it floating.

GUID-20230607-SS0I-GGXH-HNWT-WVDDPQC3HBXQ-low.svg Figure 2 General-purpose dual-supply IA with an integrated RG.

Equation 2 gives the transfer function for this circuit:

Equation 2. V O U T = V I N + - V I N - × 10 V V   o r   20 V V

Designers will typically select this IA when their requirements necessitate a balance of cost, performance and PCB area. The INA350ABSIDSGR IA was chosen for this comparison because of its affordability, performance, small package (lead DSG = WSON = 4 mm2), selectable gain (10 V/V or 20 V/V) and low typical input offset voltage (VOS(typ) = 200 µV). This implementation needs no external components. For designs that require higher gains, the INA350CDS has gains of 30 V/V or 50 V/V.

Figure 3 is a simplified schematic of the TI INA333 precision dual-supply IA with an external RG. VREF connects to ground. In this circuit, the IA integrates all resistors except RG. The differential input voltage is VIN+ − VIN– and the output voltage is VOUT. Some components, such as the load resistor (10 kΩ) and decoupling capacitors, are not shown.

GUID-20230607-SS0I-VKW3-MKVB-JZLM3D7GF5M9-low.svg Figure 3 Precision dual-supply IA with an external RG.

Equation 3 gives the transfer function for this circuit:

Equation 3. V O U T = V I N + - V I N - × 1 + 100   k Ω R G

Designers typically use a precision IA when performance is the highest priority. The INA333AIDRGR precision IA was selected for this comparison because it is low voltage (5 V), has excellent precision (G = 1 V/V, VOS(typ) = 35 µV) and comes in a small package (DRG = WSON = 9 mm2). The performance over temperature depends on the selection of the external RG. Therefore, to be consistent with the primary design priority – performance – we used a precision RG for a gain of 10 V/V (±0.05%, ±10 ppm/°C). Because the precision op amps are integrated, this implementation has excellent gain range (1 V/V to 1,000 V/V). The overall cost is usually greater than the other two solutions, however, given the integrated precision op amps and required precision RG.