SLYT844 September 2023 LMG3522R030 , TMS320F280049C
The topology uses two phases operating 180° out of phase with a single DC blocking capacitor, Cb, taking advantage of the ripple current cancellation provided by the two-phase architecture and reducing the root-mean-square (RMS) current stress in Cb. Lb1 and Lb2 are sized to process the high-frequency AC ripple current necessary for TCM operation, removing the DC bias burden required for the inductor used in TCM, as defined in [5]. Using ferrite cores for Lb1 and Lb2 ensures low loss in the presence of the high flux swings necessary for zero voltage switching (ZVS). Lg1 and Lg2 are larger in value than Lb1 and Lb2 (approximately 10 times larger), preventing most of the high-frequency current from flowing into the input source and subsequently improving EMI. In addition, the reduced ripple current in Lg1 and Lg2 enables the possible use of lower-cost core materials. Figure 1 also illustrates the ripple current envelopes for the inductors and switch nodes.