Depletion-mode MOSFETs are by default
on when MOSFET VGS is 0V, unlike enhanced-mode MOSFETs that require
VGS to be greater than the threshold voltage of the MOSFET. In order
to turn off the depletion MOSFET, VGS needs to be <0V (typical ranges
are from –1V to –4V). To analyze the effect of the depletion-mode MOSFET in an ideal
diode-sense path, let’s look at device operation under these conditions:
- When VPV–
VPV+: The ideal diode controller is in forward-condition mode,
keeping both the power MOSFET Q1 and depletion FET QD on.
With these operating conditions, you can calculate the output voltage as
VOUT = VIN – (ID_Q1
RDS(on)_Q1), approximated to VPV+.
- When VPV– < VPV+: The ideal diode controller is in the
reverse current blocking condition, with MOSFET Q1 turned off. MOSFET
QD is in regulation mode as a source follower, maintaining
VCATHODE above VANODE, VCATHODE =
VIN(VANODE)+ (VGSMAX). So the voltage
across VCATHODE to VANODE is within the absolute maximum
rating VGSMAX of QD (usually <5V), which is far less
than the maximum reverse voltage of 45V transient of the LM74610-Q1. The high
reverse voltage (VOUT – VIN) is sustained by the
drain-to-source voltage (VDS) of QD and
Q1.
Selecting the correct depletion MOSFET and power MOSFET depends on these points:
- Choose a VDS rating of Q1 and QD greater than
the maximum peak input voltage.
- Select RDS(on) such that dissipation across the power-path MOSFET is
lowest. The drain current (ID) of the FET should be higher than the
maximum peak current demanded by the output load. Selecting a depletion MOSFET
with a drop of 50mV to 100mV across the power MOSFET at the full load current is
a good starting point.
- RDS(on) can be in the
hundreds of ohms range (the LM74610-Q1’s floating gate-drive
architecture has a large impedance of cathode pin to ground, and the
ICATHODE of the controller is in the microamperes range).
Figure 5 shows test results for a 60V bypass switch solution using the 40V LM74610-Q1 controller.
With properly scaled MOSFETs (Q1 and QD), the input voltage range can
extend to the VDS rating of the FETs. This enables high-voltage designs
using the same low-voltage controller. Also, extending the input voltage range can
also be useful in enterprise, communication, power tool and high-voltage
battery-management applications.