The following instructions describe how to set up and use the TMAG5110-5111EVM:
- Power up the EVM using either of the following methods:
- USB power
- Insert the micro USB cable into the EVM onboard USB receptacle J1.
- Plug the USB cable into any USB power source (for example: laptop, desktop, power bank, and so forth).
- Variable power supply
- Set the power supply voltage to 5 V. Do not turn on the power yet.
- Connect the power supply V- terminal to the black GND test point on the EVM.
- Connect the power supply V+ terminal to the red VCC test point on the EVM.
- Turn on the power supply.
- Place either the 10 pole or the 20 pole ring magnet in one of the two positions indicated in Figure 3-3.
- Rotate the magnet in either direction and observe the various LED indicators.