SLYU055A January 2020 – November 2020 TMAG5124
Follow the procedure listed below to set up and use the TMAG5124EVM with a single 5-V supply:
1. Ensure that plug J5 is shorted.
2. Connect an external 5-V DC supply voltage to the VCC connection point. Ensure the 5-V supply is powered down for now.
3. Connect a wire from "VCC_OUT" on the control board to the "VCC_OUT" port of the TMAG5124 device to be evaluated. Repeat this process for "GND."
4. Turn on the supply. The blue "OFF" light turns on. This indicates that the device is turned on, and current is flowing through the loop.
5. Test the TMAG5124EVM as outlined in section Section 4.3 below.