SLYY231A March   2024  â€“ March 2024 BQ25171-Q1 , BQ25622 , BQ25638 , LMQ66430-Q1 , LMR36502 , TPS37-Q1 , TPS62903-Q1 , TPSM365R15

 

  1.   1
  2.   Overview
  3.   At a glance
  4.   The importance of nano-IQ in different power applications
  5.   Achieving nano IQ in industrial BMS monitors
  6.   Achieving nano IQ in automotive BMS monitors
    1.     Achieving nano IQ in industrial home automation chargers
  7.   Achieving nano IQ in automotive BMS chargers
  8.   Achieving nano IQ in voltage supervisors
  9.   Achieving nano IQ in industrial and personal electronics DC/DC converters
  10.   Achieving nano IQ in automotive DC/DC converters
  11.   Conclusion
  12.   References
  13.   Additional resources

The importance of nano-IQ in different power applications

The need to improve battery life with every device generation is increasing, driving requirements for lower IQ. These devices can be configured to work in normal mode, sleep/standby mode or shutdown mode. Normal mode only accounts for a very small portion of a power application’s mission profile [1]; these types of products are in standby mode most of the time. The current draw from the power supply can be several milliamperes in normal mode where there will be bursts of high-speed communication, and several nanoamperes when going into sleep or standby mode. Nanoampere-level working modes can conserve power to support longer battery life.

This paper discusses design mechanisms to achieve nano-IQ in different power applications such as industrial and automotive BMS battery voltage monitors, chargers, DC/DC converters and voltage supervisors, along with challenges. On one hand, nano-IQ is required to enable longer battery life; on the other hand, the integrated circuit (IC) needs to consume a certain amount of IQ to sustain functionalities such as system wakeup.